Bike Fixation Indoor Vertical Single Non-Lockable Bike Mount

Rollover image to zoom in

Click image to enlarge

See all 9 items in product family

Bike Fixation Indoor Vertical Single Non-Lockable Bike Mount

Item #: WB442814

In Stock, Ships in 3-4 Days Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

List Price: $65.56 Save up to 19%
Price: $ 52.95
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
SARIS® VERTICAL INDOOR BIKE TRAC
Bike Trac
Vertical bike racks store bicycles vertically against walls for out-of-the-way storage. Vertical bike storage racks accommodate bikes with narrow or wide wheels to accept all bicycles. Bicycle storage racks are made of durable steel. Full length tray keeps bikes in place. Mounts to wall, corner, pillar or post.

This product is Made in the USA.

Product Specifications

    • CAPACITY 1 Bike
    • COLOR FINISHBlack
    • BRANDBike Fixation by Saris®
    • CONSTRUCTIONSteel
    • DESCRIPTION1-Bike Bike Trac
    • MOUNT TYPEVertical Mount, Non-Locking
    • TYPENo Locking
    • WEIGHT LBS9 (4.09 kg)
Have A Question About This Product?
1 Question | 1 | Answer

Avg. Customer Rating: (10 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

Bike Rack Art

We have 6 of these bike racks hanging in our office reception area. Visitors, employees and vendors think it is art when bikes are hanging on it. Beautiful!!

See more favorable reviews

The most critical review

  • Customer Rating

Vertical Bike Rack

The rack is very solid and heavy. Once installed it works well except for wider off road tires. If you have a wide open space to install it and are fortunate enough to have a stud available to screw into installation would be simple. Because of its weight it only seems reasonable to use drywall toggles. Due to its shape these must be installed simultaneously along the length of the rack. An awkward business at best. So basically, it is well built but installation can be challenging under some circumstances.

See more critical reviews

Sort by: 

10 Results

Bike Rack Art

Your review: We have 6 of these bike racks hanging in our office reception area. Visitors, employees and vendors think it is art when bikes are hanging on it. Beautiful!!

Is this review helpful?

Vertical Indoor Bike Trac

Your review: great product!

Is this review helpful?

Bike rack

Your review: Was easy to install. Only downside is track for tires was not long enough for the bikes I have(6-8 inches to short, Had to add additional piece at bottom of track to keep from marking wall by rear tire.

Is this review helpful?

Space Saving

Your review: We bought three of these and installed 4x4 posts outside, about 15-18" apart with top and bottom braces, and attached these vertical bike racks to them. They look very cool and we are able to lock the bikes up (very important in the city where bikes are commonly stolen) with heavy duty steel cables through the triangle at the top of the track. We would buy these again and highly recommend them for those who are lacking space for bike storage.

Is this review helpful?

WB442814 Vertical Bike Trac

Your review: excellent quality, easy to install, economy of space, fair price, timely shipping

Is this review helpful?

Bike Rack

Your review: works great

Is this review helpful?

Vertical Bike Rack

Your review: The rack is very solid and heavy. Once installed it works well except for wider off road tires. If you have a wide open space to install it and are fortunate enough to have a stud available to screw into installation would be simple. Because of its weight it only seems reasonable to use drywall toggles. Due to its shape these must be installed simultaneously along the length of the rack. An awkward business at best. So basically, it is well built but installation can be challenging under some circumstances.

Is this review helpful?

vertical hanging bike rack

Your review: Good quality rack. I got two and am pleased with them. The channel for the bike tires could be about 10 inches longer. The lower wheel on both the bikes I have extend past the channel which results in marking the wall. I expected the channel to prevent the problem. Maybe you could make an extension available for the channel.

Is this review helpful?

Horizontal Bike rack

Your review: Rack is very well made. The attachment screws I did not use because they were not big enough! For the road bike --channel is perfect. My mountain bike tire does not seat itself to the bottom---channel could be bigger. I mounted 5 bikes all on studs. Very will satisfied

Is this review helpful?

Great product

Your review: Easily and securely installed in under an hour on old plaster walls with simple plastic anchors. Helped me regain valuable foor space and keep my bike safe. Great price, service, and delivery. I recommend to anyone who'll listen.

Is this review helpful?

Sort by: 

10 Results

There are 10 questions and 1 answers for this product.

Sort by: 

10 Results

how long is the channel? What is the interior width of the channel? Thanks.

Question Asked By: Samuel , December 18, 2014

+ View 1 Answer

Answer This Question

Sort by: 

10 Results