Blue LED Forklift Pedestrian Safety Warning Spotlight

Rollover image to zoom in

Click image to enlarge

See all 5 items in product family

Blue LED Forklift Pedestrian Safety Warning Spotlight

Item #: WB988717

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Qty Price
1-3 $109.95 ea.
4+ $85.95 ea.
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
BEST VALUE BLUE LED FORKLIFT PEDESTRIAN SAFETY WARNING SPOTLIGHT

Promote Worker & Pedestrian Safety!

When the LED Safety Warning Spotlight assembly is mounted to a forklift or other moving vehicle, it projects bright blue spot beam pattern on the floor surface. Since multiple lights can be mounted onto a single fork lift truck, the warning light spots can be seen behind or in front of the forklift. The bright light spot on the floor is clearly visible to pedestrians, machines and vehicles in the area, regardless of the ambient noise, alerting them to the nearby presence of the forklift. Traditional audio back up alarms can blend into ambient noise in the building and pedestrians can become immune to the audio warning.

Twin 5 watt solid-state, shock-resistant, Cree LED (Light Emitting Diode) lights yielding 600 lumens are enclosed in an IP68 rated housing with a UV-resistant PMMA polycarbonate lens. The LED forklift safety light uses the vehicle electrical power to operate and can be installed on the front and/or rear of any forklift, sweeper, AGV or industrial vehicle (configured for 10 Volt to 80 Volt DC input range, with reverse voltage protection). The 50,000 hour service life LED's are mounted in a rugged die-cast aluminum housing for long life. Working environment temperature is -49 to 185° F. Universal stainless steel swivel mounting bracket allows for easy installation. 1 Year Limited Warranty.

Note: Configured for 10 to 48 Volt DC input:
0.550 amps @ 12V DC
0.280 amps @ 24V DC
0.180 amps @ 36V DC
0.140 amps @ 48V DC

Documents

Documents are in PDF format

Product Specifications

    • LENGTH INCHES6-1/2 (16.51 cm)
    • WIDTH INCHES4 (10.16 cm)
    • HEIGHT INCHES4-3/4 (12.07 cm)
    • COLOR FINISHBlack
    • # LED's2
    • APPROVAL/REGULATIONSIP68
    • ASSEMBLYAssembled
    • BRANDGlobal Industrial™
    • CONSTRUCTIONDie-Cast Aluminum Housing, PMMA Lens
    • LIMITED WARRANTY1 Year
    • LUMENS600
    • MANUFACTURER PART NUMBER988717
    • MOUNTING TYPEUniversal
    • POSITION ON FORKLIFTFront and/or Rear
    • SPOT OR LIGHT BEAM COLORBlue
    • TYPELED Forklift Safety Warning Spolight
    • VOLTAGE10 - 48
    • WEIGHT LBS1.8 (.82 kg)
    • WORKING TEMPERATURE-31 to 185° F
Have A Question About This Product?
2 Question | 2 | Answer

Avg. Customer Rating: (31 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

The most critical review

  • Customer Rating

PURCHASING MANAGER

THIS WAS PURCHASE AS A SAFETY ITEM TO BE MOUNTED ON OUR LIFT TRUCKS. THEY'RE VERY BRIGHT AND APPEARS TO BE SERVING IT'S PURPOSE.

See more critical reviews

Sort by: 
1 2 ...

31 Results

Blue LED Forklift warning light

Your review: Works great.

Is this review helpful?

Maintenance Planner/Scheduler

Your review: Bright Blue light

Is this review helpful?

Purchasing Specialist

Your review: Customer Service is always a pleasure to work with.

Is this review helpful?

Maintenance Manager

Your review: Just what we needed

Is this review helpful?

Excellent Lights

Your review: We installed these and have had excellent results!

Is this review helpful?

PURCHASING MANAGER

Your review: THIS WAS PURCHASE AS A SAFETY ITEM TO BE MOUNTED ON OUR LIFT TRUCKS. THEY'RE VERY BRIGHT AND APPEARS TO BE SERVING IT'S PURPOSE.

Is this review helpful?

Blue LED Pedestrian Safety Warning Lights

Your review: We purchased these for front/rear visibility in a Warehouse that has many blind corners.

Is this review helpful?

Safety light

Your review: We have been using these lights for years and show up great on the warehouse floor.

Is this review helpful?

safety lights

Your review: Purchased these safety lights for use in an industrial business on forklifts. They are an excellent choice- high visibility and an excellent price in comparison to other similar warning lights.

Is this review helpful?

Safety Blue

Your review: We have made several safety improvements over the years that employees see as another barrier to their job. However, this improvement has had the reverse effect. Employees comment on how much safety they feel with the blue lights on the forklifts. If the forklift operator does not sound their horn, they still no that they are present due to the blue light.

Is this review helpful?

Work Exactly How They Should

Your review: Like I said, these lights work exactly how they should on our forklifts. The blue light shines bright on the floor in both incandescent and LED overhead lighting. They are especially helpful in our plant because we have electric forklifts, and they are hard to hear coming with the surrounding factory noise.

Is this review helpful?

Blue LED Forklift Pedestrian Safety Warning Spotli

Your review: bright and clear, rugged, easy to install. will repurchase as needed

Is this review helpful?

Good item

Your review: Very bright, focused beam, durable case

Is this review helpful?

Fork Lift Blue Safety Light

Your review: I had these blue lights intalled on our fork lifts and I am very happy with them. I feel as though the folks are more aware of the vehicle traffic in the warehouse now as they are noticing the blue lights on the floor as they move around.

Is this review helpful?

Safety LED Lights

Your review: A must have in the warehouse. Great addition to any lift to promote the maximum safety.

Is this review helpful?

BLUE PEDESTRIAN SAFETY LIGHT

Your review: This warning light works very well. It shines on the floor ahead of or behind the lift. When a pedestrian sees this light on the floor it make them stop and see where the light is coming from. #RP1988717 is not the brightest of this type of light that is sold. It is plenty sufficient though. An excellent value.

Is this review helpful?

Pedestrian Safety Light

Your review: Very good light to try to warn pedestrians of a forklift coming. Shines bright blue oval on floors. This model is not the brightest out there but it is plenty bright to do the job.

Is this review helpful?

Purchasing Agent

Your review: We tested this product on one of our fork trucks and the very first day it saved ME! An electric fork truck that is very quiet,I did not hear or see but, that bright blue beam was 15' ahead of it around a blind corner! I almost stepped in front of the truck. We have installed forward AND rear facing light systems to maximize the safety benefit on our 8 fork and roll clamp trucks at our commercial printing plant. So far we have been very pleased with them. It is a great safety feature for the price!

Is this review helpful?

Pedestrian warning

Your review: Alerts pedestrian about approaching forklift in a loud area.

Is this review helpful?

The Blue Light

Your review: These are a great safety item for your forklift. If you have deep aisles that you have to back out of or even backing away from a truck after loading a pallet this blue light is a great visual warning that the forklift is in reverse gear either moving or about to move. So many times you can hear the lift but not sure where it is coming from or there is multiple lifts in the area, this will allow you to pin point which lift is backing up.

Is this review helpful?

Can't miss it!!

Your review: The point of the light is to alert pedestrians of on coming lifts. Well I can see this when I drive past the facility, safe to say it works.

Is this review helpful?

Blue Safety Lights

Your review: These work great, we put one on the Front and back of our forklifts for safety. When coming out of one of our aisles, you can see the blue light on the floor prior to the forklift coming out. We made up some signs and one minute lesson on the safety blue lights. Just had our safety inspection and passed with flying colors.

Is this review helpful?

Warning LIght

Your review: Good product at a reasonable price.

Is this review helpful?

Pedestrian Safety

Your review: This light was priced right and works as designed. The build quality is high and seems to be very durable.

Is this review helpful?

Sort by: 
1 2 ...

31 Results

There are 31 questions and 2 answers for this product.

Sort by: 
1 2 ...  

31 Results

Can you provide a better price if purchasing 75+ blue lights? Also please provide warranty details for this product.

Question Asked By: Daniel Craven , Albany, Ga , September 04, 2015

+ View 1 Answer

Answer This Question

Can you provide a IP-68 certification for the forklift spotter light ?

Question Asked By: anonymous

+ View 1 Answer

Answer This Question

Sort by: 
1 2 ...  

31 Results