approx. 22K
Ladder injuries in 2020**
6-10 FT.
The most common ladder falls happen between 6 and 10 feet off the ground
$6B
$6 billion is spent on workplace falls from working at heights*
TOP 3
Falls are the 3rd most common cause for disabling workplace injury*
#3
Ladders are #3 on OSHA’s Top 10 Most Cited Violations list.***
A ladder is deemed unsafe when it is too long or too short for the job at hand. Whether it’s a Rolling platform ladder or a step ladder for climbing - make sure the length is sufficient enough to avoid standing on the top rung or step of the ladder.
Pay close attention to the ladder’s Duty Rating ― it should exceed the total weight of the climber, plus any tools, supplies, and objects placed upon its rungs or steps. Ignoring this rule can turn any safety ladder into a ladder accident.
There are many types of ladders. Step ladders have a self-supporting, hinged design that’s ideal for small projects at fixed heights. Straight & Extension ladders are adjustable and require a stable structure of support to lean on.
A rocky or unstable ladder spells trouble. Make sure it is placed on firm, level ground, without any obstructions or slippery surfaces near or around the base of the ladder. Wear slip-resistant shoes with heavy soles for added traction and support.
Climbing up or down a ladder is safest when utilizing three points of contact. This means facing the ladder and having two hands and one foot, or two feet and one hand, in contact with the ladder’s steps, rungs, and/or side rails at all times. This ladder safety tip can help reduce the risk of slips and falls.
Every March, the American Ladder Institute holds its annual National Ladder Safety Month to encourage both homeowners and employees to become familiar with ladder safety in an effort to reduce ladder-related injuries and fatalities each year. But ladder safety isn’t just a one-time-only initiative. There are a number of resources you can turn to all year long for tips, checklists, training, and more. Do Your Part
Our selection includes various types of ladders, such as step ladders, rolling ladders, step stools, extension ladders, and more, all made with high-quality materials for durability and safety. We also carry personnel lifts, including scissor lifts, boom lifts, and aerial lifts, for elevated work tasks that require mobility and accessibility. Our products are suitable for use in industrial and commercial settings, as well as for personal use. Browse our selection today to find the perfect ladder or lift for your specific needs.