Industrial Strength Steel Hand Truck with Curved Handle & Stair Climbers 600 Lb. Capacity

Rollover image to zoom in

Click image to enlarge

See all 48 items in product family

Industrial Strength Steel Hand Truck with Curved Handle & Stair Climbers 600 Lb. Capacity

Item #: WB241439

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Qty Price
1-2 $139.95 ea.
3+ $129.95 ea.
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
INDUSTRIAL STRENGTH STEEL HAND TRUCK

High quality, 1-1/4" diameter steel tube trucks are perfect for day-to-day work in warehouse, receiving and delivery. MIG welded throughout with double welding at critical stress points to withstand rugged use. Curved Handle offers easiest load control. 10" x 3-1/2" full pneumatic ball bearing wheels offer best load protection and roll smoothly over roughest surfaces. Durable enamel finish resists rust and scratches. Has a 14" x 10" noseplate, integral Stair Climbers that use continuous friction reducing belts to ease movement up and down stairs, and a 350 lb. capacity Folding 24" Nose Extension to increase bulk carrying capacity. Assembles easily. 5 Year Frame Warranty.

Click here to see our full selection of Hand Trucks & Dollies.

Documents

Documents are in PDF format

Product Specifications

    • WIDTH INCHES22 (55.88 cm)
    • HEIGHT INCHES49 (124.46 cm)
    • CAPACITY LBS600 (272.73 kg)
    • COLOR FINISHBlue
    • ASSEMBLYUnassembled
    • BRANDGlobal Industrial™
    • CONSTRUCTIONSteel
    • LIMITED WARRANTY5 Year
    • STYLEG
    • TYPECurved Handle
    • WEIGHT LBS32 (14.55 kg)
    • WHEEL DIAMETER INCHES10 (25.4 cm)
    • WHEEL TYPEPneumatic
Have A Question About This Product?
1 Question | 1 | Answer

Avg. Customer Rating: (16 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

Stair climber dolly

Good product, but stair climber tract broke. Instead of questioning me or asking me to send it back, they just refunded my full payment and told me to "dispose of the dolly" as I see fit. Needless to say, I still can use it as a normal dolly, so I'm totally blown away. I love Global and have purchased a couple of things from them in the past, and I have never been disappointed. Good company!!!

See more favorable reviews

The most critical review

  • Customer Rating

Stair climber did not work

This hand truck had great potential (we loved the large wheels and long nose) but it failed miserably on the stair climbers. When we received the units, some of the rollers that were supposed to be inside the stair climber assembly were already falling out. The belt would not turn even under a load nor would it stay tight enough to keep the rollers in place. The design is simply flawed. The stair climbers pictured look great, but that is not what came pre-installed on the units we received. That being said, their customer service was EXCELLENT and we were able to return the product at no charge to us. It's just unfortunate that the design was so poor. Hopefully that gets fixed sometime. *** Global Management Comment: Thank you for your feedback. Stair climbers have been modified to roll easier for future shipments. ***

See more critical reviews

Sort by: 

16 Results

It's a handtruck

Your review: What I needed around my house and yard.

Is this review helpful?

Pneumatic Tire Hand Truck

Your review: I Like This Hand Truck & Would Buy Another One !!

Is this review helpful?

Review Update-New stair climber hardware

Your review: 4 stars for customer services sending me the new hardware free of charge with minimal hassle. The rollers do not fall out of the new climbers and the belts do turn more easily. The design and appearance is the same. The belts do not roll like they are on a metal ball bearing track so there is still friction. Need to move a 200 lb. generator up stairs. Will see how it goes.

Is this review helpful?

Stiar Climbers Need To Be Redesigned

Your review: Maybe they modified the stair climbers to roll easier, but they sure don't roll easier on the one I purchased. I had to spray some WD40 on the belts to get them to move. One of the problems is they use a fan belt that is not made to the shape of the climber housing. This results in an overly loose fit along the lengths and a too tight fit on the ends which cause the belts to dig into the ends of the housing. The rollers fall out along the length because they are held in only by gravity and the belt tension. *** Global Comment: We have improved the stair climbers for these. All new incoming inventory will have the revised stair climbers. We also have some of the new stair climbers that were shipped to us for replacements. We will be setting those up as a replacement part ***

Is this review helpful?

Product was good

Your review: We are pleased with the product and the promptness of delivery.

Is this review helpful?

Stair climber dolly

Your review: Good product, but stair climber tract broke. Instead of questioning me or asking me to send it back, they just refunded my full payment and told me to "dispose of the dolly" as I see fit. Needless to say, I still can use it as a normal dolly, so I'm totally blown away. I love Global and have purchased a couple of things from them in the past, and I have never been disappointed. Good company!!!

Is this review helpful?

Stair climber did not work

Your review: This hand truck had great potential (we loved the large wheels and long nose) but it failed miserably on the stair climbers. When we received the units, some of the rollers that were supposed to be inside the stair climber assembly were already falling out. The belt would not turn even under a load nor would it stay tight enough to keep the rollers in place. The design is simply flawed. The stair climbers pictured look great, but that is not what came pre-installed on the units we received. That being said, their customer service was EXCELLENT and we were able to return the product at no charge to us. It's just unfortunate that the design was so poor. Hopefully that gets fixed sometime. *** Global Management Comment: Thank you for your feedback. Stair climbers have been modified to roll easier for future shipments. ***

Is this review helpful?

Steel hand truck curved handle with stair climbers

Your review: This hand truck is well-built. The curved handle is comfortable. The longer platform is easy to work with; its held up with Velcro when not needed. The price was reasonable. We're using it in our community food pantry.

Is this review helpful?

Hand Truck

Your review: Excellent hand truck. Perfect for hauling heavy loads. It is very sturdy and built to last.

Is this review helpful?

Hand truck with stair climbers

Your review: Great price and the large wheels are a plus. The product was shipped very quickly.

Is this review helpful?

Hand truck

Your review: Exactly what we were looking for and delivered in a timely manner.

Is this review helpful?

Works great but not so slick on stairs

Your review: This is a great hand truck for the money. There are two sets of holes for the axle. Choose the one farthest to the rear so that the wheels clear any items on the deck. The rear axel location will assist on stairs as well. The only aspect is that the stair belts are very stiff and do not operate well. Perhaps over time it will improve.

Is this review helpful?

Office Manager

Your review: We are extremely happy with the hand truck.

Is this review helpful?

very pleased

Your review: I love the hand truck with the stair climbers. We are moving and it was dilvered within days easy to put together. The only draw back is it's a bit heavey, however,is extremely easy to manouver

Is this review helpful?

Cart with stair climbers

Your review: this is great heavy duty nice.

Is this review helpful?

Works beautifully

Your review: This hand truck works beautifully to get items up and down stairs without the normal strain involved when having to do this. Excellent purchase. Thank you~

Is this review helpful?

Sort by: 

16 Results

There are 16 questions and 1 answers for this product.

Sort by: 

16 Results

i need a replacement stair climber part for this hand truck. is there a specific part number for this?

Question Asked By: Geoff , Malvern, PA , March 14, 2012

+ View 1 Answer

Answer This Question

Sort by: 

16 Results