Single Fork Mounted Drum Gripper 1500 Lb. Capacity

Rollover image to zoom in

Click image to enlarge

See all 37 items in product family

Single Fork Mounted Drum Gripper 1500 Lb. Capacity

Item #: WB795332

Ships same day. Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $ 386.95
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
SINGLE FORK-MOUNTED DRUM GRIPPER

Allows the operator to lift, transport, and deposit steel drums without leaving the seat of the forklift truck. Mounts easily on the forks, just hand tighten lock screws, no tools required. The knuckle gripping system is lowered around the drum, gripped tightly, and then lifted. The weight of the drum holds grab jaws in place to minimize slippage. Drum is automatically released by lowering the forks. Welded steel construction. Features hinged folding arm design to save storage space. Powder coat yellow finish. 1 Year Limited Warranty.

Product Specifications

    • CAPACITY LBS1500 (681.82 kg)
    • COLOR FINISHYellow
    • ASSEMBLYAssembled
    • BRANDGlobal Industrial™
    • CENTER TO CENTER OF FORK TINE INCHES16 (40.64 cm)
    • CONSTRUCTIONSteel
    • DESCRIPTIONSingle Drum Grab
    • DRUM GALLON55 (208.2 l)
    • FORK OPENING INCHES5-1/4 x 2
    • JAW SIZE INCHESFor 55 Gallon Drums up to 22.4" Diameter
    • LIMITED WARRANTY YEARS1 Year
    • MANUFACTURERS PART NUMBERDG-10
    • REFERENCE #DGS-55-D
    • TYPEHinged Folding Arm Design
    • WEIGHT LBS109 (49.55 kg)
Have A Question About This Product?
2 Question | 0 | Answer

Avg. Customer Rating: (15 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

Easy all the way around

Easy to store, put on forks and use. Worth every penny- no more scraped up drums from trying to use just the forks to move them. Safer for the employees as well.

See more favorable reviews

The most critical review

  • Customer Rating

Needed some modifying to work properly

When I got this item I had to shorten the stops slightly to make it fit my barrels which are just under 22 1/2" diameter. I also had to the brackets on the top side of the pivot points so that the barrel rings would not rest on this bracket while in the drum grab. After this modifications it works pretty good but does take some getting used to. It also works best on older heavier built drum. Some of my newer drums that only weigh 30 lbs empty will dent pretty easily with this unit. My older ones that weigh 60 lbs empty do not have this problem.

See more critical reviews

Sort by: 

15 Results

Easy all the way around

Your review: Easy to store, put on forks and use. Worth every penny- no more scraped up drums from trying to use just the forks to move them. Safer for the employees as well.

Is this review helpful?

1 person found this review helpful

Good for the Money

Your review: We tried this solution out before going to more expensive hydraulic route to see if we could save money. It does the job, even works on bent drums

Is this review helpful?

1 person found this review helpful

drum gripper

Your review: works just as advertised, no complaints

Is this review helpful?

drum handler

Your review: good product good price

Is this review helpful?

Drum Gripper

Your review: Very Well Made.

Is this review helpful?

Drum Gripper

Your review: This drum gripper works great. Just as advertised.

Is this review helpful?

Pretty Nifty

Your review: Our Engineers are very happy with this tool. It helps us where there is no clearance for the hanging type and that was all we were finding until we came to Global... We just love these guys

Is this review helpful?

Grabber

Your review: The grabber is well made and the forks fold back onto the frame, which is a good space saver when not in use. The only drawback so far is that the grabber does does mark/dent the drums a bit. I think that this is due to is being new and somewhat "stiff". I am hoping that with use, it will break in nicely.

Is this review helpful?

Needed some modifying to work properly

Your review: When I got this item I had to shorten the stops slightly to make it fit my barrels which are just under 22 1/2" diameter. I also had to the brackets on the top side of the pivot points so that the barrel rings would not rest on this bracket while in the drum grab. After this modifications it works pretty good but does take some getting used to. It also works best on older heavier built drum. Some of my newer drums that only weigh 30 lbs empty will dent pretty easily with this unit. My older ones that weigh 60 lbs empty do not have this problem.

Is this review helpful?

Drum gripper

Your review: The drum gripper has made our life's much easier, where it was a two man job unloading 500lbs drums now it's a simple one man job.

Is this review helpful?

Durable & simple design with great functionality!!

Your review: We move drums around about 3 times a month and did not need an overly complicated drim lift. This lift is basic and simple and stores in a small location. I am happy with the purchase.

Is this review helpful?

WQ795332 Single Fork Mounted Drum Gripper

Your review: DELIVERED AS PROMISED. EXCELLENT VALUE.

Is this review helpful?

good

Your review: It worth the money. Good results.

Is this review helpful?

Satisfied

Your review: This product seems to work well. Have only used it a couple of times since purchasing it. Very well built and functions as it should. It has the attachment point for a safety chain that I did not see on several other grippers that I looked at before purchasing this one.

Is this review helpful?

Product good shipping poor

Your review: The product survived the shipping but the shipping container took a beating.

Is this review helpful?

Sort by: 

15 Results

There are 15 questions and 0 answers for this product.

Sort by: 

15 Results

Will this work for poly and steel 55 gal drums? If not which one can work with both kinds of drums? Thank you

Question Asked By: Doug , Ohio , September 21, 2015

Not Answered Yet

Answer This Question

Does this unit work on fiber drums?

Question Asked By: Jim , April 03, 2015

Not Answered Yet

Answer This Question

Sort by: 

15 Results