Continental Fan LT100 Lint Trap
See all 6 items in product family

Continental Fan LT100 Lint Trap

Item #: WBB177931

Ships From US, Add 3-4 days For Delivery Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $ 66.95
Product Information
Customer Review
Product Q&A
Lint Trap

May be installed between the dryer and the booster fan to help reduce lint build-up in duct and maintenance to the fan. Improves drying capacity. 26 gauge corrosion resistant, satin coat steel can be painted to match decor. Mounts flush to drywall surface. Ceiling or wall mount option. 9/16" mounting flange. One piece door with intergral screen. Galvanized mesh filter. Sturdy slide mechanism is simple to use. This optional lint trap can be used with Dryer Booster Kits.

Product Specifications

    • BRANDContinental Fan
    • COLORSatin Coat
    • CONSTRUCTIONSteel with Galvanized Mesh Filter
    • DEPTH INCHES6-1/8 (15.56 cm)
    • DESCRIPTIONLint Trap
    • HEIGHT INCHES8-7/8 (22.54 cm)
    • HEIGHT RANGE1-12"
    • INLET/OUTLET DIAMETER INCHES4-1/8 Inlet 3-7/8 Outlet
    • LIMITED WARRANTY YEARS1
    • MANUFACTURER PART NUMBERLT100
    • WIDTH INCHES6-1/8 (15.56 cm)
    • WIDTH RANGE1-12"
Have A Question About This Product?
4 Question | 0 | Answer

Avg. Customer Rating: (10 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

Excellent secondary trap

My application was the vent blowing onto the roof so wanted to have a secondary filter and this provided an excellent solution.

See more favorable reviews

The most critical review

  • Customer Rating

Lint Trap

the box does not close properly causing lint and hot air to escape. We have lined the edges with rubber lining and place clips on the lid to keep it closed

See more critical reviews

Sort by: 

10 Results

Lint Trap

Your review: the box does not close properly causing lint and hot air to escape. We have lined the edges with rubber lining and place clips on the lid to keep it closed

Is this review helpful?

Excellent secondary trap

Your review: My application was the vent blowing onto the roof so wanted to have a secondary filter and this provided an excellent solution.

Is this review helpful?

lint trap

Your review: just what I needed a little pricey with shipping tax etc didn't get a chance to price sears unit

Is this review helpful?

Lint Trap

Your review: Does anyone have any ideas as to how to seal the lid to the base. It would require using some sort of gasket that is heat tolerant as the lint trap does get quite warm depending on the dryeer cycle. I also have tried to use a "clip" to hold the lid tighter to the base.

Is this review helpful?

Great trap

Is this review helpful?

Lint Trap

Your review: I installed this lint trap in a customers basement area that was unfinished. I had to fabricate a mounting bracket that would hold it to a block wall. Works great. Product photo should be upgraded to current model. It would also be nice to have direction of air flow if it makes any difference.

Is this review helpful?

Gas Dryer Lint Trap

Your review: Product is performing as expected.

Is this review helpful?

Good, simple product

Your review: I recently purchased your external Lint Trap. It was exactly what I expected. It was easy to install and seems to be working great.

Is this review helpful?

Lint Trap

Your review: Item arrived quickly and packaged very well. Will use Global again

Is this review helpful?

lint trap

Your review: Very good value. Installed easily. Very effective for stopping lint that gets past the lint trap that is inside the dryer. Easy to remove and clean the screen. The unit I received is not exactly as pictured in the photo. Mine has no window in the door like the photo seems to show. Also, the screen, which is shown diagonally inside the metal box, separate from the door, is actually welded directly to the inside of the door. This welded design probably makes removing the screen for cleaning much easier.

Is this review helpful?

Sort by: 

10 Results

There are 10 questions and 0 answers for this product.

Sort by: 

10 Results

Does this product have to be installed in an upright position

Question Asked By: Michael , December 26, 2014

Not Answered Yet

Answer This Question

Someone asked the question but it was not directly answered. Can this be used with a GAS dryer?

Question Asked By: scott , December 26, 2014

Not Answered Yet

Answer This Question

My question is two-fold. Can this trap be used with a gas dryer? The outlet lines for the dryer vent run in the garage in a protected enclosure on the floor. Can the trap be mounted on the floor with the trap "door" facing up? Thanks in advance for your help.

Question Asked By: Michael , home , February 27, 2013

Not Answered Yet

Answer This Question

can I use this as a final lint trap for an indoor residential dryer?

Question Asked By: Eddie , November 29, 2011

Not Answered Yet

Answer This Question

Sort by: 

10 Results

Customers Who Viewed This Also Viewed