Buyers Products Electric Trailer Tongue Jack 3025539 3500 Lb. Capacity

Rollover image to zoom in

Click image to enlarge

Buyers Products Electric Trailer Tongue Jack 3025539 3500 Lb. Capacity

Item #: WB985400

Usually ships in 3 to 6 days Estimated lead times do not include weekends or holidays. Transit time is determined by shipping method and destination. Orders requiring credit information might take additional time.

Price: $230.95
Product Information
Photo/Video Gallery
Customer Review
Product Q&A
Accessories
Buyers Products ELECTRIC TRAILER JACK

Battery Powered Jack offers a Fast and Easy Method to Hitch and Level Trailers.

This 12V DC jack is powered by your tow vehicles battery to offer quick, effortless lifting in 30 seconds. Innovative features include an integral level at the top of the jack for easy leveling and dual LED lights to help with nighttime coupling. Hardened steel gears allow for 3500 lb. lifting capacity and 5000 lb. breakaway capacity to assist with ball release. Jack offers a full 24" of stroke (18" of power lift; 6" manual drop leg extension), universal bolt pattern A-Frame coupler mounting flange, weather-sealed operating switch and manual crank override when battery power is not available. Detachable zinc-plated foot is adjustable on 1-½"H intervals and an oversized 5-¼" diameter foot pad prevents divots. Durable black powder-coat wrinkle finish.

Mounting Plate is 5-1/4" diameter overall; Hole slots are 3/4" x 7/16" on a 3" radius.

Product Specifications

    • LENGTH INCHES6.9 (17.53 cm)
    • WIDTH INCHES6-1/4 (15.88 cm)
    • HEIGHT INCHES26-1/2 (67.31 cm)
    • CAPACITY LBS.3500 Lift; 5000 Breakaway
    • COLOR FINISHBlack
    • ASSEMBLYAssembled
    • BOLT SPACINGHole slots are 3/4" x 7/16" on a 3" radius
    • BRANDBuyers Products
    • CONSTRUCTIONSteel
    • LIFTING RANGE INCHES24 (Powered 18; Manual Drop Leg Extension 6)
    • MANUFACTURERS PART NUMBER3025539
    • MOUNT TYPEA-Frame (5-1/4" diameter overall)
    • VOLTAGE12
    • WEIGHT LBS.19 (8.64 kg)
Have A Question About This Product?
0 Question | 0 | Answer

Avg. Customer Rating: (7 customer reviews)

Write your own review

The most favorable review

  • Customer Rating

Electric trailer tongue jack

This is an excellent jack for the money. I highly reccomend Global to anyone. The only issue I had was the jack plug had to be rewired to work on my 2006 GMC Sierra factory install receptacle. I called Global to explain that the jack was not working for me and they quickly delivered another jack. After discovering the 2nd jack did not work either I realized I needed to look at the wiring. Originally I did not want to start disassembling anything for fear of voiding any warranty. It was a fairly simple fix. Thank you Global and a special thanks to Susan Hooper and the other young ladies I spoke with.

See more favorable reviews

The most critical review

  • Customer Rating

So Far, So Good

I installed this jack on a trailer with a 600 lb tongue weight. It lifts the weight just fine. The only negative thing I can see so far is that it is pretty slow. I guess they had to gear it low to lift the maximum rating. Still beats a manual crank.

See more critical reviews

Sort by: 
1 ...

7 Results

So Far, So Good

Your review: I installed this jack on a trailer with a 600 lb tongue weight. It lifts the weight just fine. The only negative thing I can see so far is that it is pretty slow. I guess they had to gear it low to lift the maximum rating. Still beats a manual crank.

Is this review helpful?

Electric trailer tongue jack

Your review: This is an excellent jack for the money. I highly reccomend Global to anyone. The only issue I had was the jack plug had to be rewired to work on my 2006 GMC Sierra factory install receptacle. I called Global to explain that the jack was not working for me and they quickly delivered another jack. After discovering the 2nd jack did not work either I realized I needed to look at the wiring. Originally I did not want to start disassembling anything for fear of voiding any warranty. It was a fairly simple fix. Thank you Global and a special thanks to Susan Hooper and the other young ladies I spoke with.

Is this review helpful?

Quick, Easy, works well

Your review: Right out of the box we had good luck with these jacks. I bought two, one each for our equipment trailers. Tongue weight between 500 and 1500 pounds. They moved a little slower than I thought but then again, they are moving a good load. Still faster than spinning the old jacks and no more busted knuckles.

Is this review helpful?

electric tongue jack

Your review: You didn't have the one I ordered but you had a white one on hand and wanted to know if I could use a white one,I said the color didn't matter as long as it worked . I recieved it the next day.Thank you for the fast service. 5 stars all the way.

Is this review helpful?

very good jack

Your review: this jack does everything as described and was well pleased with its performance, it was not hard to to install, i have not had any problems

Is this review helpful?

trailer tongue jack 3500 lb. capacity

Your review: The jack work outstanding and I would have purchase another one if I had another trailer.

Is this review helpful?

wb985400 electric trailer jack

Your review: the jack works good easy to install no problems well worth the money

Is this review helpful?

Sort by: 
1 ...

7 Results