Browse O-Rings & Seals

(1,388 items)

Narrow Your Results

Length Inches

Width Inches

Depth Inches

  • Less...
  • More...

Recently Viewed

Categories

  • Rod Wiper - D Style

    Rod Wiper - D Style
    See all 34 items in product family
    The main function of the Rod Wiper is to keep the rod and cylinder clean and free from foreign matter; thus preventing premature failure. The Rod Wiper is not a pressure sealing element, yet it avoids possible abrasive effects which may result if contaminants were to reach the sealing and rod bearing elements.

    One-piece snap-in type rod wiper scrapers for heavy duty applications. WD (RWD) wipers are continuous (not split) and conform with wear and side motion for effective wiping action over the entire life span of the seal.

    Click for more
  • Rod Wiper - AN Style

    Rod Wiper - AN Style
    See all 31 items in product family
    The main function of the Rod Wiper is to keep the rod and cylinder clean and free from foreign matter; thus preventing premature failure. The Rod Wiper is not a pressure sealing element, yet it avoids possible abrasive effects which may result if contaminants were to reach the sealing and rod bearing elements.

    Designed for light duty applications where style WD wipers are not required. Interchangeable with corresponding dash numbers of MS28776 wiper rings.

    Click for more
  • Piston Cups

    Piston Cups
    See all 28 items in product family
    Piston Cups are primarily used on piston heads, plungers or rams in hydraulic or pneumatic service. Its mechanical sealing surface is at its periphery. Piston Cups are commonly used because of economical cost, excellent service life, efficient assemble, universal acceptance, and simple accessories.

    Fabric reinforced Piston Cups prevent extrusion in medium pressure installations (up to 1000 psi) or where diametrical clearances are greater.

    Click for more
  • U Cup - AN Style

    U Cup - AN Style
    See all 21 items in product family
    U-Cups derive their name from their shape and are self-sealing on both the inside diameter and outside diameter. They are most often used for sealing rams or rods and are very popular due to the small gland space required. They are especially adapted to low speed, low pressure environments for both pnuematic and hydraulic cylinders. They provide an extremely smooth, steady movement because of their inherent low friction.

    The seal is obtained by means of the flared, flexible lips coming in contact with the rod or cylinder wall. Clearance is provided at the heel for minimum friction. Through this design, the packing is preloaded when installed. Sealing effectiveness is increased by internal pressure of the air or fluid against the inner surface of the lips. For continued sealing effectiveness and long seal life, the surface finish of the working surface of either rods or bores should be a maximum of 16 microinches. It is not recommended that U-cups or any other single lip seal be used in any application where there is excessive side loading.

    The 6226 Series U-Cup has a flat sealing lip and is available in 70 Durometer Nitrile.

    The lips of the U-Cup should always be toward the pressure force. The U-Cup is a floating seal which means the height of the U-Cup should be between .015" to .090" shorter than the depth of the gland. (See the Packing Space Chart below). The added gland space allows the pressure to equalize on both lips, thus keeping the U-Cup from rolling. The surface finish for a static seal surface should be 32 RMS maximum. The dynamic surface should be in the range of 8 to 16 RMS. Finishes rougher than 16 RMS could cause premature lip wear and finishes finer than 8 RMS can result in failure of the seal due to loss of lubrication.

    Click for more
  • Standard Lip Seal

    Standard Lip Seal
    See all 69 items in product family
    Standard Lip Seals Are Designed To Improve Performance Of Rods Or Pistons..

    Standard Lip Seals are molded from 92 Durometer Urethane with a 70 Durometer Nitrile energizer. The energizer ensures constant pressure on the sealing lips. Energizing the sealing lips with an endless O-ring assures uniform, positive lip contact and excellent low pressure sealing. Seal depth is equal to the radial width, which results in a square design. Can be widely used to interchange with existing hydraulic packing and/or O-rings without changing dimensions. Available in a wide range of 3/8 to 5-/4 inch diameters of various dimensional sizes.

    Click for more
  • Rod Wiper - H Style

    Rod Wiper - H Style
    See all 11 items in product family
    The main function of the Rod Wiper is to keep the rod and cylinder clean and free from foreign matter; thus preventing premature failure. The Rod Wiper is not a pressure sealing element, yet it avoids possible abrasive effects which may result if contaminants were to reach the sealing and rod bearing elements.

    Designed for medium duty applications and can provide both wiping and sealing action in one component in low pressure systems. The external lip scrapes foreign matters from the rod, and the other lips act as an effective pressure seal in low pressure applications. This wiper can also be used as a secondary seal to trap slight leakage from the primary seal. This creates a very dry rod system. The WH Rod Wiper is also known as Series 8600.

    Click for more
  • Type B Lip Seal

    Type B Lip Seal
    See all 48 items in product family
    Loaded Lip Seals are very versatile and can be used as rod seals or piston seals. They are considered to be multi-purpose seals and are designed for significantly improved performance. These Loaded Lip Seals are molded from 92 Durometer Urethane with a 70 Durometer Nitrile energizer. The energizer ensures constant pressure on the sealing lips.

    The Loaded Lip Seal Type "B" features a back-beveled sealing lip. This provides greater film breaking and increased unit loading at the sealing surface. The seal depth is generally 1 1/2 times the radial width to ensure seal stability in the most rugged applications. It is most commonly used as a rod seal.

    Click for more
Featured Items